Does the MIMXRT1060-EVKB contain a camera?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the MIMXRT1060-EVKB contain a camera?

816 Views
anonymous3957
Contributor I

EDIT: This is quite urgent for me! Please help me ASAP

According to the MIMXRT1060-EVKB Board User Manual, it contains:

- MIMXRT1060-EVKB board

- USB Type A to micro-B cable

- Camera, CA111C based on MT9M114

but looking at this unboxing, I just can't spot it. On the Packing List shown in the video, there are actually 3 components:

- 700-47858: PWA, MIMXRT1060-EVKB

- 600-77315: USB 2.0 TO MICRO 1.0M

- 926-79035: QSG, MIMXRT1060-EVKB

but I just see the Board and the USB cable in the video. So maybe one of two Product Numbers which isn't the USB cable is supposed to be the camera (even though I don't see it)? I can't find any information regarding those PNs on the internet.

0 Kudos
Reply
1 Reply

754 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @anonymous3957 ,

   About the RT board situation, you can find it from the website:

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1060-eva...

kerryzhou_0-1659346399276.png

kerryzhou_1-1659346406700.png

 

I find the EVK contains the camera, but the EVKB didn't list it.

So, the MIMXRT1060-EVKB should don't have it.

If you still have questions about it, you can contact with the side where you buy the board, if it is distributor, check with distributor, if it is the NXP web, you can check with:

direct@nxp.com

 

Wish it helps you!

Best Regards,

kerry

 

0 Kudos
Reply