Does NXP provide tool to test i.MXRT10xx SDRAM timing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP provide tool to test i.MXRT10xx SDRAM timing?

Jump to solution
1,544 Views
ffloree
Contributor III

As title, I remembered that NXP has a tool named like DDRx_test to verify i.MX6 ddr timing, but does RT10xx have?

Tags (1)
1 Solution
1,332 Views
igorpadykov
NXP Employee
NXP Employee

Hi tom

unfortunately such tool is not available for i.MXRT.

MCUXpresso has evkmimxrt1020_sdram_ini_dcd.c,SDRAM_Init() in evkmimxrt1020_sdram_init.jlinkscript,
examples which may be useful.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,333 Views
igorpadykov
NXP Employee
NXP Employee

Hi tom

unfortunately such tool is not available for i.MXRT.

MCUXpresso has evkmimxrt1020_sdram_ini_dcd.c,SDRAM_Init() in evkmimxrt1020_sdram_init.jlinkscript,
examples which may be useful.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,332 Views
ffloree
Contributor III

thank you

0 Kudos
Reply