Difference of lite and non-lite source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference of lite and non-lite source code

1,715 Views
sathishkumar_r
Contributor II

Hi,

May I know the pros and cons of using the lite source code(evkmimxrt1060_dev_video_virtual_camera_lite_bm) & non-lite source code(evkmimxrt1060_dev_video_virtual_camera_bm) which is provided in SDK example for RT1060?

Thanks in advance...

Labels (1)
1 Reply

1,656 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Sathish,

When you download the SDK from the SDK builder you will see an option named "Download SDK Documentation". If you download this file, in the path docs/USB you will find a pdf file named "MCUXpresso SDK USB Stack Device Reference Manual". Section 1.1 of this document explains the differences between lite and non-lite.

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------