Device Tree issues with the iMXRT devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device Tree issues with the iMXRT devices

1,173 Views
jautry
Contributor IV

I am working on bringing a new design using the iMXRT1062 proc with an embedded linux platform. I am having some issues with setting up the device tree for an audio device, particularly the clocks. Are there any device tree examples around for the iMXRT devices? I usually only see stuff for the iMX6

Tags (1)
0 Kudos
Reply
3 Replies

1,168 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Are there any device tree examples around for the iMXRT devices? I usually only see stuff for the iMX6
-- Before answering your question, I'd like to know whether you will use the Zephyr OS in the new design, if not, it doesn't need the device tree actually.
Suppose you will use Zephyr OS, please go to download the Zephyr OS for the NXP platform.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,156 Views
jautry
Contributor IV

I am not using Zephyr but am using uClinux

Tags (1)
0 Kudos
Reply

1,144 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1)Are there any device tree examples around for the iMXRT devices?
-- Unfortunately, the NXP hasn't provided the example demos for the uClinux until now.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply