Hello,
in the reference manual rev3. from 07/2021 on page 208 it says that PFD_480_PFD1 is selected as clock source for the Flexspi at boot time for nor flash.
If i read the registers for flexspi mux and div i find the values 3 and 4. Mux value 3 means kCLOCK_Usb1PllPfd0Clk is the clock source. If i use Clock_GetFreq(kCLOCK_Usb1PllPfd0Clk) the value is 480 * 18 / 13 MHz. This divided by 5 is near 133 MHz for the nor flash. 133 MHz is also the clock value for my flash.
I can't find a possible clock mux value of PLL3 PFD1 (PFD_480_PFD1) for the Flexspi.
Is this an error in the reference manual?
Best regards,
kalimanni