DSP Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP Clock

1,891件の閲覧回数
adc_6_6
Contributor III

Is it possible to operate the Fusion F1 DSP integrated in the RT595 at a different clock frequency than the M33?

For instance, having the M33 run at 100 MHz and the DSP at 50 MHz.

Thank you.

タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,869件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @adc_6_6,

 

The PLL of RT595 provides an alternate high-frequency clock source for the Fusion DSP CPU if the required frequency is different from the main system clock.

You can see the clock distribution in the chapter 6 called "Clock Control" in the Reference manual. Additionally, config tools could be help you switch to these frequencies.

 

Also, if you experience any issue, do not hesitate to let me know.

BR

Habib.

0 件の賞賛
返信

1,820件の閲覧回数
adc_6_6
Contributor III

Hello @Habib_MS

Thank you for your response.

I understand that it is possible to operate at different clocks.

Is there anything specific I need to be particularly careful about in this case?

0 件の賞賛
返信

1,783件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello again @adc_6_6,

Does not exist a particular specification that you have be careful. Only remember that the maximum clock frequency of both is 200MHz, as shown the next diagram:

Habib_MS_0-1719432226913.png

Also, if you experience any issue, do not hesitate to let me know.

BR

Habib.

1,768件の閲覧回数
adc_6_6
Contributor III
Hello @Habib_MS
Thank you for your response.
0 件の賞賛
返信