DMA controller uses the APBH bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA controller uses the APBH bus

1,526件の閲覧回数
danbocko
Contributor I

Anyone have examples or starter code for the I.MX287 to use SSP with the DMA controller and the APBH bus. I am trying to read an 8-channel ADC and store the values using DMA. Working in RTOS instead of Linux.

Thanks

Dan

タグ(2)
0 件の賞賛
返信
1 返信

1,386件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dan

unfortunately I am not aware of i.MX28 spi baremetal examples, may be useful to

check uboot patch on:

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信