DCDC corrupts USB in IMXRT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DCDC corrupts USB in IMXRT1170

跳至解决方案
1,781 次查看
Juozas
Contributor III

Dear forum,

We've noticed strange behaviour using MIMXRT1176 chip. When we set DCDC 1P0 buck target to 1.35V (kDCDC_1P0BuckTarget1P325V) or higher using DCDC_SetVDD1P0BuckModeTargetVoltage() function, USB stops working correctly. We're not sure what's wrong – my guess is something with USB clocks.

Is this a software or a hardware bug? Our project specification requires using internal DCDC with 1P0 buck target 1.35V and higher.

Regards

0 项奖励
回复
1 解答
1,771 次查看
lucas_cao
NXP Employee
NXP Employee

The 1.325V out of the absolute max rating

lucas_cao_0-1674097334451.png

 

在原帖中查看解决方案

2 回复数
1,772 次查看
lucas_cao
NXP Employee
NXP Employee

The 1.325V out of the absolute max rating

lucas_cao_0-1674097334451.png

 

1,761 次查看
Juozas
Contributor III

Thank you, we should select another chip for this project.

0 项奖励
回复