DCDC corrupts USB in IMXRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DCDC corrupts USB in IMXRT1170

Jump to solution
1,713 Views
Juozas
Contributor III

Dear forum,

We've noticed strange behaviour using MIMXRT1176 chip. When we set DCDC 1P0 buck target to 1.35V (kDCDC_1P0BuckTarget1P325V) or higher using DCDC_SetVDD1P0BuckModeTargetVoltage() function, USB stops working correctly. We're not sure what's wrong – my guess is something with USB clocks.

Is this a software or a hardware bug? Our project specification requires using internal DCDC with 1P0 buck target 1.35V and higher.

Regards

0 Kudos
Reply
1 Solution
1,703 Views
lucas_cao
NXP Employee
NXP Employee

The 1.325V out of the absolute max rating

lucas_cao_0-1674097334451.png

 

View solution in original post

2 Replies
1,704 Views
lucas_cao
NXP Employee
NXP Employee

The 1.325V out of the absolute max rating

lucas_cao_0-1674097334451.png

 

1,693 Views
Juozas
Contributor III

Thank you, we should select another chip for this project.

0 Kudos
Reply