DCD file update on IMX RT 1176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DCD file update on IMX RT 1176

738 Views
tbayram
Contributor IV

Hello,

We are working on a custom board with an IMX RT 1176 processor. The external RAM is different from the SDRAM used on the EVK. There are two 32MB SDRAMs on the EVK and one 4MB SDRAM on the custom board. Because of these differences, I need to make changes to the DCD file. How can I modify the DCD file? Can the DCD be updated using the SEMC peripheral? I need to modify the DCD file of any RGB project. Can you help me to do DCD file update or DCD file update via SEMC?

 

Thanks.

0 Kudos
Reply
3 Replies

724 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @tbayram ,

    Except the memory size difference, any other difference or not?

   If just the memory size difference, it is easy to modify it, you just need to change the size in the project memory:

kerryzhou_0-1707193101755.png

But, if totally the different flash, then you need to modify the DCD, and before you do the DCD modification, I highly recommend you run this SDK demo and do the modification at first:

SDK_2_14_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\semc\sdram\cm7

Mainly modify this code:

status_t BOARD_InitSEMC(void)
{
    semc_config_t config;
    semc_sdram_config_t sdramconfig;
    uint32_t clockFrq = EXAMPLE_SEMC_CLK_FREQ;

    /* Initializes the MAC configure structure to zero. */
    memset(&config, 0, sizeof(semc_config_t));
    memset(&sdramconfig, 0, sizeof(semc_sdram_config_t));

    /* Initialize SEMC. */
    SEMC_GetDefaultConfig(&config);
    config.dqsMode = kSEMC_Loopbackdqspad; /* For more accurate timing. */
    SEMC_Init(SEMC, &config);

    /* Configure SDRAM. */
    sdramconfig.csxPinMux           = kSEMC_MUXCSX0;
    sdramconfig.address             = 0x80000000;
    sdramconfig.memsize_kbytes      = 2 * 32 * 1024;       /* 64MB = 2*32*1024*1KBytes*/
    sdramconfig.portSize            = kSEMC_PortSize32Bit; /*two 16-bit SDRAMs make up 32-bit portsize*/
    sdramconfig.burstLen            = kSEMC_Sdram_BurstLen8;
    sdramconfig.columnAddrBitNum    = kSEMC_SdramColunm_9bit;
    sdramconfig.casLatency          = kSEMC_LatencyThree;
    sdramconfig.tPrecharge2Act_Ns   = 15; /* tRP 15ns */
    sdramconfig.tAct2ReadWrite_Ns   = 15; /* tRCD 15ns */
    sdramconfig.tRefreshRecovery_Ns = 70; /* Use the maximum of the (Trfc , Txsr). */
    sdramconfig.tWriteRecovery_Ns   = 10; /* tWR 10ns */
    sdramconfig.tCkeOff_Ns =
        42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/
    sdramconfig.tAct2Prechage_Ns       = 40; /* tRAS 40ns */
    sdramconfig.tSelfRefRecovery_Ns    = 70;
    sdramconfig.tRefresh2Refresh_Ns    = 60;
    sdramconfig.tAct2Act_Ns            = 10;                  /* tRC/tRDD 10ns */
    sdramconfig.tPrescalePeriod_Ns     = 160 * (1000000000 / clockFrq);
    sdramconfig.refreshPeriod_nsPerRow = 64 * 1000000 / 8192; /* 64ms/8192 */
    sdramconfig.refreshUrgThreshold    = sdramconfig.refreshPeriod_nsPerRow;
    sdramconfig.refreshBurstLen        = 1;
    sdramconfig.delayChain             = 6; /* For all tempeatures. */
    sdramconfig.autofreshTimes = 8; /* An additional eight Auto Refresh cycles (CBR) are also required before or after
                                       programming the Mode Register to ensure proper subsequent operation. */

    return SEMC_ConfigureSDRAM(SEMC, kSEMC_SDRAM_CS0, &sdramconfig, clockFrq);
}

memsize_kbytes=> to your real used memory side:
sdramconfig.tPrecharge2Act_Ns = 15; /* tRP 15ns */
sdramconfig.tAct2ReadWrite_Ns = 15; /* tRCD 15ns */
sdramconfig.tRefreshRecovery_Ns = 70; /* Use the maximum of the (Trfc , Txsr). */
sdramconfig.tWriteRecovery_Ns = 10; /* tWR 10ns */
sdramconfig.tCkeOff_Ns =
42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/
sdramconfig.tAct2Prechage_Ns = 40; /* tRAS 40ns */
sdramconfig.tSelfRefRecovery_Ns = 70;
sdramconfig.tRefresh2Refresh_Ns = 60;
sdramconfig.tAct2Act_Ns = 10; /* tRC/tRDD 10ns */
sdramconfig.tPrescalePeriod_Ns = 160 * (1000000000 / clockFrq);
sdramconfig.refreshPeriod_nsPerRow = 64 * 1000000 / 8192; /* 64ms/8192 */

The above parameter, you need to refer to your used SDRAM datasheet to modify it.
Then do the testing, make sure all the SDRAM data write and read is correct.

After this works, then you can modify the dcd.c:

kerryzhou_1-1707193594133.png

Mainly fill the SDRAMCRn register to the data which you tested in the above semc_cm7 demo.

You can try it on your side.

If you still have a question about it, please kindly let me know.

Wish it helps you!

Best Regards,

Kerry

 

 

 

0 Kudos
Reply

715 Views
tbayram
Contributor IV
hi @kerryzhou,
How can I change pins on dcd file? Because evk has 2 SDRAM and I must close SEMC A12 and SEMC_D16 to SEMC_D31.
0 Kudos
Reply

711 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @tbayram ,

In the first area of the DCD.c, it is the SEMC pin control:

kerryzhou_0-1707211854555.png

 

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply