Could maestro audio play support output bit depths 32 bits ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could maestro audio play support output bit depths 32 bits ?

ソリューションへジャンプ
759件の閲覧回数
antoniohsu888
Contributor II

I use mp3 with sampling rate 32k Hz and bit depths 32 bits to test the maestro mp3 deocde.

It will decode the mp3 to sampling rate 32k Hz and bit depths 16 bits.

Is it possible force it to decode the bit depths to 32 bits ?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
755件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @antoniohsu888 

  From the maestro lib description, the mp3 decode just support 16 bits, not 32bits.

kerryzhou_0-1661147756458.png

So, to the 32bit depth mp3, maybe you need to switch it to the 16depth at first.

 

Wish it helps you!

Best Regards,

kerry

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
756件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @antoniohsu888 

  From the maestro lib description, the mp3 decode just support 16 bits, not 32bits.

kerryzhou_0-1661147756458.png

So, to the 32bit depth mp3, maybe you need to switch it to the 16depth at first.

 

Wish it helps you!

Best Regards,

kerry

 

0 件の賞賛
返信