Connecting 8MB Flash and 8MB PSRAM to one FlexSPI[portA/B] interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting 8MB Flash and 8MB PSRAM to one FlexSPI[portA/B] interface

1,105 Views
bharatgohil
Contributor I

Hi,

We are developing custom board with IMXRT101x uC. Can we connect 8MB(8-pin SOIC) flash and 8MB(8-pin SOIC) PSRAM(ESPRAM or IPUS PSRAM) to FlexSPI portA[0:3] and port portB[3:0] respectively? We want access both the interface together.

if yes, How PSRAM will be access and what is base address of PSRAM?

Regards,

Bharat 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,065 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Bharat, 

Is not possible to connect two different types of memories to the same FlexSPI interface. If your application needs an external RAM then I would suggest you migrate to the RT1020. The RT1020 besides the FlexSPI interface it has an interface called SEMC (Smart External Memory Controller) which supports external RAM memories. 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 Kudos
Reply

1,065 Views
bharatgohil
Contributor I

Thank You Vector.

Got it.

Regards,

Bharat

0 Kudos
Reply