Complete toolchain with standard libraries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Complete toolchain with standard libraries

1,072 次查看
jakobczyk_woj
Contributor I

I'm trying to build my project on my build server.

I have prepared a makefile and it runs ok on my local machine, when using SDK installed in MCUExpresso IDE (my toolchain is at /usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/arm-none-eabi/)

However, on my build machine I don't want to install the IDE, so I'm using a gcc-enabled SDK built in the MCU Xpresso SDK Builder and an ARM toolchain downloaded from developer.arm.com.

My problem is that the toolchain does not include some of the libraries used in the project, such as libm, libstdc++_nano or libcr_newlib_semihost.
These libraries are available in the SDK installed from the IDE.

How can I get these without installing the IDE?

My board is iMX RT1051 and the project is bare metal.

0 项奖励
回复
2 回复数

1,056 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @jakobczyk_woj ,

Maybe you can install MCUXpresso on another computer and then copy those files to your system.

 

Regards,

jing

0 项奖励
回复

1,039 次查看
jakobczyk_woj
Contributor I

Well, sure, but it's kind of a workaround, not a proper solution. There should be a way to build the project without installing IDE, especially as there is a download for gcc-based MCU SDK.

0 项奖励
回复