Communication protocol between IMX8 and RT1052

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Communication protocol between IMX8 and RT1052

Jump to solution
183 Views
jiaxin
Contributor I

Hi,sir

Requirements:
The system requires data interaction between RT1052 and IMX8, and the wider the rate, the better

What is the maximum bandwidth communication mode between imx8 and RT1052?

0 Kudos
Reply
1 Solution
103 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The bandwidth will depend on the protocol used for communication.
You can opt to use LPSPI or ethernet for the communication between devices. 

Best regards,
Omar

View solution in original post

0 Kudos
Reply
2 Replies
104 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The bandwidth will depend on the protocol used for communication.
You can opt to use LPSPI or ethernet for the communication between devices. 

Best regards,
Omar

0 Kudos
Reply
151 Views
jiaxin
Contributor I

The amount of data each interaction between the two chips is 512 bytes, and the less time spent, the better

0 Kudos
Reply