Code execution from Flash on i.MX RT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code execution from Flash on i.MX RT1064

2,379件の閲覧回数
sivaram_grps
Contributor I

We are checking i.MX RT1064 for our future product, we would like to know if we need external RAM for code execution, or the code can be directly executed from on chip flash. 

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,085件の閲覧回数
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 件の賞賛
返信

2,085件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sivaram

yes code can be directly executed from on chip flash.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,085件の閲覧回数
carstengroen
Senior Contributor II

Igor,

what is the penalty/performance if executing from the 4 MB internal flash on the 1064 ?

(I know its probably hard to give a precise answer, I'm more after a "rule of thumb" regarding this)

0 件の賞賛
返信

2,085件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sivaram

I think performance is the same as with externally connected flash.

Best regards
igor

0 件の賞賛
返信