Can the iMXRT1170 support 2 cameras?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the iMXRT1170 support 2 cameras?

Jump to solution
1,835 Views
EdSutter
Senior Contributor II

Subject says it all...

I have a small compact design coming up that needs two cameras.  Can the 1170 support two?

 

0 Kudos
Reply
1 Solution
1,830 Views
kerryzhou
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
1,822 Views
EdSutter
Senior Contributor II

Ok thanks for the pointer.  Seems at best it would be a bit of a kludge to do a 2-camera design then...

0 Kudos
Reply
1,831 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EdSutter ,

Please check this post:

https://community.nxp.com/t5/i-MX-Processors/Two-camera-input-on-i-MX-RT1170/m-p/1356235#M181597

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply