Can the FLEXSPI Driver API Perform a SPI Transfer without the LUT ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can the FLEXSPI Driver API Perform a SPI Transfer without the LUT ?

1,017件の閲覧回数
mjpovi
Contributor III

This question may have been somewhat answered, but I want to ask if the FLEXSPI driver API can or cannot do a SPI transfer without using the LUT ?  If it can do a transfer without using the LUT, is there any example code for that ?

Thanks!

0 件の賞賛
返信
1 返信

1,008件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @mjpovi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) This question may have been somewhat answered, but I want to ask if the FLEXSPI driver API can or cannot do an SPI transfer without using the LUT ?
-- No, I'm afraid not.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信