Can I use ST-Link V2 to program the smart voice board(SLN-SVUI-IOT)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use ST-Link V2 to program the smart voice board(SLN-SVUI-IOT)?

874 Views
AndryckSant
Contributor II

Hello community,

 

I am trying to flash the micropython firmware on NXP's smart voice board(SLN-SVUI-IOT). It is a board project based on another board, the MiMXRT1060.

 

I realized that in the Smart Voice's schematics, it does not have an onboard debugger. I was wondering if I can use an original ST-Link V2 to program the smart voice board and flash the micropython firmware. I also noted that the "STM32" port of the ST-Link has a 20 pin JTAG port. The smart voice board has a 10 pin JTAG port. I can use some kind of adapter on it?

 

Or I was also wondering if I could use a specific hardware with the daplink firmware to program the board. Here is the link of the hardware mentioned: https://pt.aliexpress.com/item/1005005634441693.html?spm=a2g0o.productlist.main.1.78d4205f4bniF9&alg...

Labels (1)
0 Kudos
Reply
2 Replies

856 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can use the debugger on MXRT.

Regards

0 Kudos
Reply

851 Views
AndryckSant
Contributor II

I think this board does not have a debugger.

 

I'm with a Smart Voice board(SLN-SVUI-IOT)

 

please, take a look at its schematics.

 

best regards, 

Andryck Santiago

0 Kudos
Reply