Can I interface IP camera through Ethernet in i.MX RT 1176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I interface IP camera through Ethernet in i.MX RT 1176

800 Views
avikumar
Contributor I

Hi,

As I have explored till now I don't find any examples related Ethernet based camera interface.

   is it possible to interface  Ethernet based camera? 

    if Yes please guide me to stream through  Ethernet based camera.

 

Thanks

Avi kumar

0 Kudos
Reply
2 Replies

785 Views
avikumar
Contributor I

Thanks.

 

0 Kudos
Reply

792 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

You should be able to receive the IP camera stream on the i.MXRT1170. There is not an example with the IP Camera implementation per se. However, the i.MXRT1170 SDK has some Ethernet and lwip examples, which may help as a starting point.

Regards,
Victor 

0 Kudos
Reply