CMSIS NN library for MCUXpresso SDK 2.11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS NN library for MCUXpresso SDK 2.11

ソリューションへジャンプ
1,266件の閲覧回数
yf2
Contributor III

Dear support,

I noticed that the CMSIS NN library is missing in $SDK/CMSIS/ folder of v2.11 SDK.

How could I add the missing CMSIS NN library to this SDK?

It seems that the CMSIS library shipped with SDK v2.11 is close to v5.6.0 version of CMSIS on Github, but the version in SDK might already have some improvements or bugfixing.

Can we simply grab the NN library in the CMSIS v5.6.0 Github release? I am wondering why SDK owner don't do it if it is that simple.

 

Regards,

yf2

タグ(1)
0 件の賞賛
返信
1 解決策
1,236件の閲覧回数
CarlosGarabito
NXP TechSupport
NXP TechSupport

We recently update the SDK and MCUXpresso IDE, some bug was eliminated, so check it this error was clean

Have a good day

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,237件の閲覧回数
CarlosGarabito
NXP TechSupport
NXP TechSupport

We recently update the SDK and MCUXpresso IDE, some bug was eliminated, so check it this error was clean

Have a good day

0 件の賞賛
返信
1,234件の閲覧回数
yf2
Contributor III

@CarlosGarabito 

Did you mean that SDK v2.12 has CMSIS-NN included by default?

I manually added CMSIS-NN to SDK as a sibling folder of DSP/ and Core/, so far no issues have been noitced yet.

Regards,

yf2

0 件の賞賛
返信
1,230件の閲覧回数
yf2
Contributor III

@CarlosGarabito 

I just downloaded a copy of SDK v2.12 and noticed that CMSIS/NN folder exists.

Will close this ticket.

yf2

 

タグ(1)