CANNOT find the device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CANNOT find the device

8,168 次查看
YaChun
Contributor I

I have been using "NXP MCU Boot Utility v3.5.0" with USB serial downloader to flash images on to the device.


But now cannot find the device, with HAB status is closed after
I using the secure Boot Type OTFAD Encrypted Image Boot & change the existing certificate.

 

0 项奖励
回复
7 回复数

8,157 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to the above attachments, it seems that you already enabled the HAB secure boot of the MCU before, so I'd like to know whether the MCU BootUtility tool retains the corresponding key and SRK table.
Have a great day,t
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

8,154 次查看
YaChun
Contributor I

Found in the directorys...

But I change the key by clicking "Generate Certificate, SRK" many times, and choose not using the existing...

0 项奖励
回复

8,135 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
According to your statement, it seems like the corresponding key and SRK table are missing or overlapped, if yes, it's impossible to sign the flashload or application image as the application note shows.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复

8,129 次查看
YaChun
Contributor I

Could I use some command like "mass erase"?

0 项奖励
回复

8,122 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Could I use some commands like "mass erase"?
-- No, I'm afraid that it's impossible to disable the HAB authentication function via some commands.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

8,119 次查看
YaChun
Contributor I

But i didn’t change any parameter, just clicking the "Generate Certificate, SRK" button, why the key changing or missing?

By the way, the  application note i can't open, does it has name that i  can search?

0 项奖励
回复

8,104 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
As mentioned before, you already enabled the HAB secure boot of the MCU, then to enter the Serial Download mode, it's essential to assure the MCUBootUtility retains the corresponding key and SRK table, just as the post shows,
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复