C++ linker in a C project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C++ linker in a C project

ソリューションへジャンプ
2,007件の閲覧回数
rubensjunior
Contributor IV

Dear collegues,

Is it possible to use a C ++ linker in a C project? If so, how do I configure it on MCUXpresso?

Thanks a lot, best regards.

Rubens Júnior

ラベル(1)
1 解決策
1,937件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Rubens,

 

What is recommended is to create a new C++ project from the project wizard and include your files to it.

 

Best regards,

Felipe

元の投稿で解決策を見る

2 返答(返信)
1,938件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Rubens,

 

What is recommended is to create a new C++ project from the project wizard and include your files to it.

 

Best regards,

Felipe

1,937件の閲覧回数
rubensjunior
Contributor IV

Felipe,

Thank you very much! Best regards.

Rubens

0 件の賞賛
返信