Hello,
we're having some issues in performing a boundary scan on our board based on i.MXRT1175. It looks like the scan correctly connects but the connection falls down after a while, not allowing us to complete the test.
We've tried the test also on MIMXRT1170-EVK, but the result is the same.
We've followed AN12919 (Introduction to Boundary Scan of i.MX RT Series) and i.MXRT1175 bsdl indicates the following compliance pins pattern:
(TEST_MODE, GPIO_LPSR_13, POR_B, ONOFF) (0011)
but there's no way to complete the boundary scan.
In another board we've developed that's based on i.MXRT1062 we've no problem in performing the test.
Is anybody able to complete the boundary scan on i.MXRT1170 family? What are we missing?
Thanks,
Antonio