Hello René,
For BOOT_MODE1 and BOOT_MODE0, use one of these options to achieve logic 0:
• Tie to GND through any-value external resistor
• Tie directly to GND
A value of 4.7 kohm is preferred for high-noise environments.
For further information I highly recommend you to check the i.MX RT Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor.
Hope it helps!
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------