Azure RTOS support for I.MX RT102x with MCUXpresso SDK.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Azure RTOS support for I.MX RT102x with MCUXpresso SDK.

785 Views
arimendes
Contributor III

Hi,

 I would like to know when NXP will support Azure RTOS with MCUXpresso SDK for I.MX RT102x. 

Will NXP license Azure RTOS for all NXP microcontrollers families, including LPC55XX?

0 Kudos
Reply
1 Reply

770 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

SDK release 2.9.1 is now available, expanding this support to incorporate the full range of i.MX RT10xx MCUs. Our team is also working with Microsoft on the LPC5500 series of devices to support Azure RTOS in the near future.

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 Kudos
Reply