Are there any speed test/comparison fetching from different memories?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there any speed test/comparison fetching from different memories?

ソリューションへジャンプ
3,656件の閲覧回数
EdSutter
Senior Contributor II

I'm writing an application with hardware that has external spi flash essentially the same as the Teensy4.1.  I'm running out of room on internal memory for text, so I'm moving some functions into xip-serial nor flash and now I'm noticing some of my realtime stuff is failing terribly.  Is there any data that shows the performance hit between execution from ITCM vs OCRAM vs SDRAM vs XIP-serial-flash (or a subset thereof)? 

Follow up question: Obviously the slowest interface is the xip-serial-flash, so is it reasonable to disable i-Cache on ITCM/OCRAM so that it is maximized on the external memories?

Thanks,

Ed 

0 件の賞賛
返信
1 解決策
3,638件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Cache can only boost OCRAM and external memory, no effect on TCM.

Disabling Cache on OCRAM may be helpful to external memory, but it is hard to quantize the effect.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,555件の閲覧回数
stephenschwartz
Contributor II

@jay_heng Tab 3 on page 14 'RT1176 - Cortex M4 core: Memory data throughput in MB/s' seems to be missing from the pdf. Would you be able to post that table? Thanks!

0 件の賞賛
返信
3,639件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Cache can only boost OCRAM and external memory, no effect on TCM.

Disabling Cache on OCRAM may be helpful to external memory, but it is hard to quantize the effect.

0 件の賞賛
返信
3,635件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Yes, you can refer to this post https://community.nxp.com/t5/RT-4-Digit-10xx-11xx-12xx/iMXRTxxxx-Memory-Performance-ITCM-DTCM-L1-CAC...

I have also attached the pdf version in case you cannot access the post