Anyone connect a OV5640 to an RT1062?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anyone connect a OV5640 to an RT1062?

108 Views
johnblackburn
Contributor II

I'm seeing some online sources stating that the RT1062 can support an OmniVision OV5640 using the DVP interface. The signaling is a little different than the DVP on the EVK for the OV7225. Has anyone successfully used a 5640 sensor on a iMXRT1062 before? What pinout did you use?

0 Kudos
Reply
2 Replies

89 Views
johnblackburn
Contributor II

Yes but the 1170 EVK uses the MIPI interface for the CSI, while the 1062 uses DVP. The DVP pins are called out on the connector of the 1170EVK, but don't connect to the processor. I'm just trying to make sure I hook up to the right pins on the processor on my 1062 since some of the naming conventions are different (HREF instead of HSYNC, XCLK instead of MCLK, etc)

0 Kudos
Reply

90 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @johnblackburn,

The RT1170-EVKB has a connector design for the OV5640, so you can use it as reference for your RT1062. You can find the schematics for the following link: https://www.nxp.com/webapp/Download?colCode=MIMXRT1170-EVKB-DESIGNFILES

BR,
Edwin.

0 Kudos
Reply