An equivalent circuit of GPIO_EMC about RT1021

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

An equivalent circuit of GPIO_EMC about RT1021

ソリューションへジャンプ
1,648件の閲覧回数
Edgard
Contributor III

Dear an Engineer in NXP,

I would like to know the equivalent circuit of GPIO_EMC pin.
Because I want to check the input mechanism.

Recently, GPIO_EMC_41 was broken, I think the electrical over stress (EOS) occurred to the pin.
I will put the 100 ohm resister close to pin in order to protect the pin from EOS.

But I wonder if the value of resister is large or not...

Thanks in advance.

Kindest Regards 
Edgard



ラベル(1)
0 件の賞賛
返信
1 解決策
1,556件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Edgard,

Application Note AN5078 describes everything relating the pins on our MCUs. With respect to ESD and EMC protection, please look into AN10853.

BR,
Edwin.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,543件の閲覧回数
Edgard
Contributor III

Hi @EdwinHz 

thanks, I checked the App.Note you mentioned.

Kindest Regards
 Edgard

0 件の賞賛
返信
1,557件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Edgard,

Application Note AN5078 describes everything relating the pins on our MCUs. With respect to ESD and EMC protection, please look into AN10853.

BR,
Edwin.

0 件の賞賛
返信