Hi,
I add a led indicator into evkmimxrt1060_tensorflow_lite_kws example, the led will light up when people say "right", or "left".
I add some config in BOARD_InitPins():
/* GPIO configuration of USER_LED on GPIO_AD_B0_09 (pin F14) */
gpio_pin_config_t USER_LED_config = {
.direction = kGPIO_DigitalOutput,
.outputLogic = 0U,
.interruptMode = kGPIO_NoIntmode
};
/* Initialize GPIO functionality on GPIO_AD_B0_09 (pin F14) */
GPIO_PinInit(GPIO1, 9U, &USER_LED_config);
GPIO_PinWrite(GPIO1, 9U, 0U);
When I write 0U to the led PIN, the led don't light up.
But if I run the blinky example, and then run kws example with my modified code, the led light up as I expect.
Please explain to me what is happening, thanks in advanced.
已解决! 转到解答。
Hello,
This behavior that you are facing might be because you are missing some configurations in the evkmimxrt1060_tensorflow_lite_kws example. This is why when you run first the other example, the project starts working properly. I guess that you are missing the configurations in the IOMUX registers in the TensorFlow project.
Regards,
Victor
Hello,
This behavior that you are facing might be because you are missing some configurations in the evkmimxrt1060_tensorflow_lite_kws example. This is why when you run first the other example, the project starts working properly. I guess that you are missing the configurations in the IOMUX registers in the TensorFlow project.
Regards,
Victor