Accessing 1-wire device using FlexIO block

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accessing 1-wire device using FlexIO block

ソリューションへジャンプ
1,439件の閲覧回数
James12
Contributor II

My MCU is RT1052 and now I need to access a temperature sensor DS18B20 which is a device with 1-wire protocal. The method of using delay function to access the 1-wire protocol is not suitable in the case of RTOS.

From the reference manual, 1-wire protocal is a typical application case for FlexIO block. But I cannot find an example of FlexIO accessing the 1-wire devide.

Anyone have such kind of example?

 

0 件の賞賛
返信
1 解決策
1,407件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @James12,

Sadly, there is not an example to work with 1-wire protocol. Nonetheless, it could be useful to check the following information of an implementation for a Kinetis microcontroller:

Best regards, Raul.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,408件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @James12,

Sadly, there is not an example to work with 1-wire protocol. Nonetheless, it could be useful to check the following information of an implementation for a Kinetis microcontroller:

Best regards, Raul.

0 件の賞賛
返信