Can the low power mode be enabled with an empty ROM?
If so, is there a description of the settings in the IMXRT1021RM?
For example, system idle mode settings.
Thank you.
Hi @hiro8235
low power mode enter need to use the code, you can download it to the internal RAM instead of the external flash, I think your mentioned empty ROM is no code in the external flash, right?
If yes, you can download this SDK code to the RAM, just not do the POR, the low power code will help you enter the low power mode.
\SDK_2_11_0_EVK-MIMXRT1020\boards\evkmimxrt1020\demo_apps\power_mode_switch
SDK download link is:
https://mcuxpresso.nxp.com/en/builder?hw=EVK-MIMXRT1020
Wish it helps you!
Best Regards,
Kerry
Hi Kerry.
Thank you for your reply.
OK, I will try to SDK code to the RAM.
Best Regards,
Hiro
Hi @hiro8235
You are welcome!
If you meet any issues, just let me know.
If your question is solved, please help to mark the correct answer, just to close this case, any new issues, welcome to create the new question post!
Best Regards,
kerry