Hi community,
I have questions about i.MX RT106F (Oasis Lite).
If you know anything, it would be greatly appreciated if you could teach me.
I am considering i.MX RT106F (Oasis Lite) for face recognition.
Q1: Could you please send me the specifications(any documentation) of Oasis Lite?
Q2: Will Oasis Lite be charged for commercialization? Is there a royalties on the device?
Q3: Is there an evaluation board that supports Oasis Lite (face recognition) and has an external interface(UART)?
*SLN-VIZNAS-IOT has no external interface(UART).
Q4: What is the recognition rate when you put a mask on your face?
Q5: What was the recognition rate when wore glasses?
Q6: How many faces can be registered with SLN-VIZNAS-IOT?
Q7: Please tell me the parameters that can be adjusted when face recognition is performed.
Q8: Is freertos the only supported OS for Oasis Lite? Do you support other OS?
Best Regards,
T.I.
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Q1: Could you please send me the specifications(any documentation) of Oasis Lite?
-- Please go to download it via the below link.
https://github.com/NXP/viznas_elock_oobe/tree/main/viznas_facereg_manager_app/doc
Q2: Will Oasis Lite be charged for commercialization? Is there a royalties on the device?
-- Yes, however, the fee already is contained in the price of the RT106F.
Q3: Is there an evaluation board that supports Oasis Lite (face recognition) and has an external interface(UART)?
*SLN-VIZNAS-IOT has no external interface(UART).
-- You can use the SLN-VIZNAS-IOT and the SLN-VIZNAS-IOT provides the UART pins on RT Vision board.
Q4: What is the recognition rate when you put a mask on your face?
-- It hasn't supported to recognize the person that wears a mask.
Q5: What was the recognition rate when wore glasses?
-- The recognition rate keeps the same, no matter whether a person wears a glass.
Q6: How many faces can be registered with SLN-VIZNAS-IOT?
-- Please refer to the following figure.
Q7: Please tell me the parameters that can be adjusted when face recognition is performed.
-- Please refer to the document that you apply for in the Q1.
Q8: Is freertos the only supported OS for Oasis Lite? Do you support other OS?
-- Oasis Lite can work with other RTOS.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------