About generated bin file size on IMXRT1176

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About generated bin file size on IMXRT1176

跳至解决方案
1,347 次查看
nxbg
Contributor I

Hi Team,

 

We are now link the project to SDRAM and execute from SDRAM(0x81600000) on IMXRT1176, then we will also use OCRAM which write speed is much faster than SDRAM.

 

So we added Extra linker script input sections to define area into OCRAM range:0x20240000 and its type is BSS, but the generated bin files will increasing to more than 1GB, this is definitely wrong.

So how can fix this problem?

Thanks & Best Regards,

 

标记 (1)
0 项奖励
回复
1 解答
1,341 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think I need more information, so I was wondering if you can describe the modification you did with the linker file in detail.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,340 次查看
nxbg
Contributor I

Hi, we find another solution to fix this problem, just close it first

0 项奖励
回复
1,342 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think I need more information, so I was wondering if you can describe the modification you did with the linker file in detail.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复