AVB-Endpoint on evk-MIMXRT1180 , RT1189_cm33 or RT1189_cm7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AVB-Endpoint on evk-MIMXRT1180 , RT1189_cm33 or RT1189_cm7

273 次查看
Sinai
Contributor I

Hi,

I am trying to build and run AVB-Endpoint on the evk-MIMXRT1180 platform.
Either on the Cortex-m33 or Cortex-m7 processor.
I think this should be possible, as the platfrom has hardware support for audio processing.
Can you confirm this?

I am working with the following software packages;

    --genavb-sdk-6_3_3 

    --SDK_2_16_000_MIMXRT1180-EVK

    -- genavb-apps-freertos-6_3_3      <-- here we got the examples 

The examples doesnt contain AVB-Endpoint for MIMXRT1180-EVK,
however when i research the MIMXRT1180-EVK SDK and compare it with MIMXRT1170-EVK SDK.
i think it should be possible for MIMXRT1180-EVK to run AVB-Endpoint only the sdk doesn't contain the functionalities yet , like for example fsl_anatop_ai.c file in the MIMXRT1170 SDK, which enables writting and reading audio data fom and to PLL registers.
we dont have this file or functionalities in MIMXRT1180-EVK SDK yet, but deeper investigation shows me that i can add this functions myself.

Can you give me more information/insight about this?


Thank You
Best Regards
Sinai    

0 项奖励
回复
2 回复数

234 次查看
Sinai
Contributor I

Hi EdwinHz,

I am working in Bosch Netherlands and we have preorderd this boards and even received a sample one to work with,
I will get back to you with the Business Relations and Queries. 

0 项奖励
回复

253 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sinai,

Since the RT1180 is still in preproduction and therefore not yet public, we are not able to provide you with information about this product on the public community forum just yet. Please contact your NXP representative (DBM) that provided you with this device for the latest information about the AVB endpoints on the RT1180.

Sorry for the inconvenience and thank you for your understanding.

BR,
Edwin.

0 项奖励
回复