AN12781 where is nn_quantizer.py ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN12781 where is nn_quantizer.py ?

905件の閲覧回数
mtx512
Contributor V

in AN12781 it mentions:

It is recommended to use the nn_quantizer.py python script available with this document in the /Scripts folder.

Which /Scripts it is referring to too as there is not attached source code ?

 

 

 

0 件の賞賛
返信
1 返信

887件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, please check the attachment.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信