关于i.mxRT600

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于i.mxRT600

4,752 Views
mycan12345
Contributor II

您好

1,最近看到rt600有密码加速器(Cryptographic Accelerator (CASPER)),发现密码加速器中有乘法器和加法器,请问一下这些算术加速器是有符号运算还是无符号运算的,例如乘法器是有符号乘法器还是无符号乘法器

2,还要rt600的powerquad中关于IIR的运算精度需要怎么计算,如下图res和ref分别代表什么??pastedImage_1.png

Labels (1)
0 Kudos
Reply
3 Replies

4,626 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

非常感谢使用NXP产品,很高兴为你提供技术支持!
1) 例如乘法器是有符号乘法器还是无符号乘法器?
-- 无符号。
2) 还要rt600的powerquad中关于IIR的运算精度需要怎么计算,如下图res和ref分别代表什么??
-- Res: 实际得出的值,Ref: 标准值(或者理论值)

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,626 Views
mycan12345
Contributor II

Hi 

不太明白关于powerquad iir精度的计算,是否可以举个计算的实例,这个理论值和实际值是否和int32,int16,fp有关??

0 Kudos
Reply

4,626 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

IIR滤波器的性能评价指标(如SNR:信噪比),说实话,我们也不是很了解,建议你自己去参考数字信号处理相关的书籍。

在SDK中也有PowerQuad关于IIR的测试代码,你也可以运行测试一下。

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply