i.MX RT Crossover MCUs Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT Crossover MCUs Knowledge Base

Discussions

Sort by:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342717 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/community/imx/blog/2019/04/17/do-you-have-a-minute 
View full article
This document describes how to use I2S (Inter-IC Sound Bus) and DMA to record and playback audio using NXP's i.MX RT600 crossover MCUs. It also includes the process of how to use the codec chip to process audio data on the i.MX RT600 Evaluation Kit (EVK) based on the Cadence® Tensilica® HiFi4 Audio DSP. Click here to access the full application note.
View full article
This document describes how to program a bootable image into the recovery Flash device using i.MX RT600 MCUs. Click here to access the full application note.
View full article
The i.MX RT600 MCU includes a Cadence® Tensilica® HiFi 4 DSP running at frequencies of up to 600 MHz.The XOS embedded kernel from Cadence is designed for efficient operation on embedded system built using the Xtensa architecture. Although various parts of XOS continue to be tuned for efficient performance on the Xtensa hardware, most of the code is written in standard C and is not Xtensa-specific. Click here to access the full application note.
View full article
This application note describes how to develop an audio player with NXP i.MX RT600 crossover MCU family. Click here to access the full application note.
View full article
The i.MX RT600 crossover MCU combines an ultra-low power MCU with a high performance DSP to enable the next generation of ML/AI, voice and audio applications. Get started today and order your MIMXRT685-EVK.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341317
View full article
This is the recording of the Crossover Code challenge Webinar presented on December 10.
View full article
Slides from webinar hosted by NXP on Dec 10, 2019.
View full article
Source code: https://github.com/JayHeng/NXP-MCUBootUtility 【v2.1.0】 Features: > 1. [RTyyyy] Support for loading bootable image into SEMC NOR boot device >     [RTyyyy] 支持下载Bootable image进主动启动设备 - SEMC NOR接口Flash > 2. [RTyyyy] Support operation under both CM7 and CM4 of RT117x A0 >     [RTyyyy] 在RT1170无论是CM7还是CM4作为主核下均能正常工作 > 3. [RTyyyy] Support two FlexSPI map addresses for RT117x A0 >     [RTyyyy] 支持RT1170的两个FlexSPI XIP映射地址 > 4. [RTyyyy] Support efuse memory operation for RT117x A0 >     [RTyyyy] 支持RT1170的eFuse回读与烧写 > 5. [RTyyyy] Can import user fuse table file to set efuse value >     [RTyyyy] 支持导入用户fuse配置文件去设置fuse > 6. [RTyyyy] Enable OTFAD encryption secure boot mode (User Key) for RT117x A0 >     [RTyyyy] 为RT1170 A0开启OTFAD加密(User Key)支持 > 7. [RTyyyy] Support RT1170/1010 bootable image from SDK as source input >     [RTyyyy] 支持RT1170/RT1010 SDK生成的Bootable image作为源文件输入 Improvements: > 1. [RTyyyy] Image format auto detection can be used for axf file from MCUX or GCC >     [RTyyyy] 程序格式自动检测选项也可用于MCUX生成的axf格式源文件 > 2. Specify file path instead of file to save readback data >    指定目录而不是指定文件去存放回读的数据 > 3. If readback data is enabled to be saved in file, then it will not displayed on the screen >    如果回读的数据已经选择保存到文件中,那么点击Read按钮将不会在窗口显示数据 Bugfixes: > 1. 'Cmd Pads' is not set correctly for some typical octal-flash models in FlexSPI NOR configuration >     在FlexSPI NOR配置界面里,对于一些octal-flash模型,其Cmd Pads参数没有被正确设置 > 2. 'Max Frequency' option is not exactly aligned with selected MCU device in FlexSPI NOR configuration >     在FlexSPI NOR配置界面里,Max Frequency参数选项与当前MCU型号不完全匹配 > 3. [RTyyyy] Cannot show total size of SD/eMMC correctly, so SD/eMMC cannot be programmed >     [RTyyyy] SD/eMMC总容量未能正确显示,导致无法编程SD/eMMC > 4. [RTyyyy] Some fields are not aligned with selected MCU device in Flexible User Key Setting >     [RTyyyy] 在用户自定义Key设置界面里,有些选项与当前选中的MCU型号不匹配 > 5. [RTyyyy] Cannot generate bootable image when original image size is less than 4KB >     [RTyyyy] 当输入的源image文件大小小于4KB时,生成可启动程序会失败 > 6. [RTyyyy] Sometimes tool cannot recognize .axf format from MCUX or Keil MDK >     [RTyyyy] 有时候无法识别MCUX或Keil MDK生成的axf格式源文件 > 7. [RTyyyy] Signed flashloader cannot be generated if DCD is enabled >     [RTyyyy] 当DCD使能的时候,无法生成含签名的Flashloader > 8. [RTyyyy] Cannot mark DCD in readback image if it comes from source bootable image >     [RTyyyy] 如果DCD来自源Bootable image,则无法在读回的image中标记DCD Interests: > 1. Add sound effect (Contra) >    增加魂斗罗音效
View full article
Overview of i.MX RT1050         The i.MX RT1050 is the industry's first crossover processor and combines the high-performance and high level of integration on an applications processors with the ease of use and real-time functionality of a micro-controller. The i.MX RT1050 runs on the Arm Cortex-M7 core at 600 MHz, it means that it definitely has the ability to do some complicated computing, such as floating-point arithmetic, matrix operation, etc. For general MCU, they're hard to conquer these complicated operations.         It has a rich peripheral which makes it suit for a variety of applications, in this demo, the PXP (Pixel Pipeline), CSI (CMOS Sensor Interface), eLCDIF (Enhanced LCD Interface) allows me to build up camera display system easily Fig 1 i.MX RT series           It has a rich peripheral which makes it suit for a variety of applications, in this demo, the PXP (Pixel Pipeline), CSI (CMOS Sensor Interface), eLCDIF (Enhanced LCD Interface) allows me to build up camera display system easily Fig 2 i.MX RT1050 Block Diagram Basic concept of Compute Vision (CV)          Machine Learning (ML) is moving to the edge because of a variety of reasons, such as bandwidth constraint, latency, reliability, security, ect. People want to have edge computing capability on embedded devices to provide more advanced services, like voice recognition for smart speakers and face detection for surveillance cameras. Fig 3 Reason        Convolutional Neural Networks (CNNs) is one of the main ways to do image recognition and image classification. CNNs use a variation of multilayer perception that requires minimal pre-processing, based on their shared-weights architecture and translation invariance characteristics. Fig 4 Structure of a typical deep neural network         Above is an example that shows the original image input on the left-hand side and how it progresses through each layer to calculate the probability on the right-hand side. Hardware MIMXRT1050 EVK Board; RK043FN02H-CT(LCD Panel) Fig 5 MIMXRT1050 EVK board Reference demo code emwin_temperature_control: demonstrates graphical widgets of the emWin library. cmsis_nn_cifar10: demonstrates a convolutional neural network (CNN) example with the use of convolution, ReLU activation, pooling and fully-connected functions from the CMSIS-NN software library. The CNN used in this example is based on the CIFAR-10 example from Caffe. The neural network consists of 3 convolution layers interspersed by ReLU activation and max-pooling layers, followed by a fully-connected layer at the end. The input to the network is a 32x32 pixel color image, which is classified into one of the 10 output classes. Note: Both of these two demo projects are from the SDK library Deploy the neuro network mode Fig 6 illustrates the steps of deploying the neuro network mode on the embedded platform. In the cmsis_nn_cifar10 demo project, it has provided the quantized parameters for the 3 convolution layer, so in this implementation, I use these parameters directly, BTW, I choose 100 images randomly from the Test set as a round of input to evaluate the accuracy of this model. And through several rounds of testing, I get the model's accuracy is about 65% as the below figure shows. Fig 6 Deploy the neuro network mode Fig 7 cmsis_nn_cifar10 demo project test result The CIFAR-10 dataset is a collection of images that are commonly used to train ML and computer vision algorithms, it consists of 60000 32x32 color images in 10 classes, with 6000 images per class ("airplane", "automobile", "bird", "cat", "deer", "dog", "frog", "horse", "ship", "truck"). There are 50000 training images and 10000 test images. Embedded platform software structure         After POR, various components are initialized, like system clock, pin mux, camera, CSI, PXP, LCD and emWin, etc. Then control GUI will show up in the LCD, press the Play button will display the camera video in the LCD, once an object into the camera's window, you can press the Capture button to pause the display and run the model to identify the object. Fig8 presents the software structure of this demo. Fig 8 Embedded platform software structure Object identify Test The three figures present the testing result.   Fig 9 Fig 10 Fig 11 Furture work          Use the Pytorch framework to train a better and more complicated convolutional network for object recognition usage.
View full article
In case you missed our recent webinar, you can check out the slides and comment below with any questions.
View full article