i.MXRT1050 SDRAM Clock Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MXRT1050 SDRAM Clock Configuration

i.MXRT1050 SDRAM Clock Configuration

  1. The path of SDRAM Clock in Clock Tree

                According CCM clock tree in i.MXRT1050 reference manual, we can abstract part of SDRAM clock, and draw it’s diagram below.

pastedImage_4.png 

  1. Descriptions for Diagram 1

(1) PLL2 PFD2

pastedImage_5.png               

① Registers related to PLL2 PFD2

---CCM_ANALOG_PLL_SYSn (page 767, in reference manual)

Address: 0x400D_8030h

important bits:

bit[15:14]---- select clock source.

Bit[13] ----- Enable PLL output

Bit[0]------- This field controls the PLL loop divider. 0 - Fout=Fref*20; 1 - Fout=Fref*22.

---CCM_ANALOG_PLL_SYS_NUM(page 768, in reference manual)

Address: 0x400D_8050h

important bits:

bit[29:0]--- 30 bit numerator (A) of fractional loop divider (signed integer)

---CCM_ANALOG_PLL_SYS_DENOM (page 769, in reference manual)

Address: 0x400D_8060h

important bits:

bit[29:0]---- 30 bit Denominator (B) of fractional loop divider (unsigned integer).

 

---CCM_ANALOG_PFD_528n (page 769, in reference manual)

Address: 0x400D_8100h

important bits:

bit[21:16]----- This field controls the fractional divide value. The resulting frequency shall be 528*18/PFD2_FRAC where PFD2_FRAC is in the range 12-35.

 

Computational formula

PLL2_PFD2_OUT=(External 24MHz)*(Fout + A/B) * 18/ PFD2_FRAC

 

③ Example for PLL2_PFD2_OUT computation

CCM_ANALOG_PLL_SYSn[0] = 1  // Fout=Fref*22

CCM_ANALOG_PLL_SYS_NUM[29:0] = 56  // A = 56

CCM_ANALOG_PLL_SYS_DENOM[29:0] = 256  // B=256

CCM_ANALOG_PFD_528n[21:16] = 29                       // PFD2_FRAC=29

 

PLL2_PFD2_OUT = 24 * (22 + 56/256)*18/29 = 331MHz (330.98MHz)

 

(2) Clock Select Register : CCM_CBCDR

Address: 0x 400F_C014h

important bits: SEMC_ALT_CLK_SEL & SEMC_CLK_SEL & SEMC_PODF

bit[7] --- bit[SEMC_ALT_CLK_SEL]

0---PLL2 PFD2 will be selected as alternative clock for SEMC root clock

1---PLL3 PFD1 will be selected as alternative clock for SEMC root clock

pastedImage_6.png

Bit[6] --- bit[SEMC_CLK_SEL]

0----Periph_clk output will be used as SEMC clock root

1----SEMC alternative clock will be used as SEMC clock root

pastedImage_7.png

Bit[18:16] --- bit[SEMC_PODF]

Post divider for SEMC clock.

NOTE: Any change of this divider might involve handshake with EMI. See CDHIPR register for the

handshake busy bits.

000 divide by 1

001 divide by 2

010 divide by 3

011 divide by 4

100 divide by 5

101 divide by 6

110 divide by 7

111 divide by 8

pastedImage_8.png

  1. Example for configuration of SDRAM Clock

 

Example : 166MHz SDRAM Clock

 

---- 0x400D8030 = 0x00002001 // wirte  0x00002001 to CCM_ANALOG_PLL_SYSn

---- 0x400D8050 = 0x00000038 // write 0x00000038 to CCM_ANALOG_PLL_SYS_NUM

---- 0x400D8060 = 0x00000100 // write 0x00000100 to CCM_ANALOG_PLL_SYS_DENOM

---- 0x400D8100 = 0x001d0000 // write 0x001d0000 to CCM_ANALOG_PFD_528n

---- 0x400FC014 = 0x00010D40 // write 0x00010D40 to CCM_CBCDR, divided by 2

 

 

 

 

NXP TIC team

Weidong Sun

2018-06-01

标签 (1)
无评分
版本历史
最后更新:
‎05-31-2018 09:16 PM
更新人: