Updating Firmware via USB DFU Based on RT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating Firmware via USB DFU Based on RT1170

Updating Firmware via USB DFU Based on RT1170

Updating Firmware via USB DFU Based on RT1170

Updating Firmware via USB DFU Based on RT1170
       
Development Environment
       
Preparing dfu-util
                
Steps to Prepare dfu-util
       
Running the Demo
                
Using Prebuilt Firmware from SDK
                
Using Custom Firmware

Performing microcontroller (MCU) firmware upgrades in the field without the aid of external programming tools is a necessary feature.
For MCUs that support USB device controllers, the USB Device Firmware Update (DFU) class offers a solution. the USB_DFU bootloader requires only a PC and a USB cable.

The RT series also provides this feature. In the case of the RT1170, for example, a DFU project is provided in the SDK under the USB class. The project is based on the MCUXpresso IDE. by running the dev_dfu_freertos_cm7 project in the SDK, the RT1170 will be enumerated as a dfu device, and after connecting it to the Host PC via another USB cable, the user can use the “dfu-util” utility to download a firmware to this device.

Development Environment

Software Environment:

  • SDK Version: 2.15.000
  • IDE: MCUXpresso IDE
  • Demo Project: dev_dfu_freertos_cm7
  • Host Software: dfu-util
    • Download link: dfu-util
    • For Windows 64-bit: Download dfu-util-0.9-win64.zip

 

Hardware Environment:

  • Board: RT1170-EVKB

 

Preparing dfu-util

dfu-util is used to download Firmware to a DFU device, but it does not add CRC32 to the Firmware. Since the DFU demo in the SDK verifies the CRC32 to ensure the Firmware written to Flash is free from bit errors, modifications to the dfu-util source code are necessary.

Steps to Prepare dfu-util

  1. Install Dependencies
  • sudo apt-get build-dep libusb-1.0-0 dfu-util
    sudo apt-get install gcc-mingw-w64-x86-64
  1. Download dfu-util and libusb Source Code
  1. Modify CRC Code in Source
    Modify the
    dfu_store_file function in dfu_file.c to add CRC32 to the Firmware suffix.
  • /* write suffix, if any */
    if (write_suffix) {
        uint8_t dfusuffix[DFU_SUFFIX_LENGTH];
        dfusuffix[0] = file->bcdDevice & 0xff;
        dfusuffix[1] = file->bcdDevice >> 8;
        dfusuffix[2] = file->idProduct & 0xff;
        dfusuffix[3] = file->idProduct >> 8;
        dfusuffix[4] = file->idVendor & 0xff;
        dfusuffix[5] = file->idVendor >> 8;
        dfusuffix[6] = file->bcdDFU & 0xff;
        dfusuffix[7] = file->bcdDFU >> 8;
        dfusuffix[8] = 'U';
        dfusuffix[9] = 'F';
        dfusuffix[10] = 'D';
        dfusuffix[11] = DFU_SUFFIX_LENGTH;
        /*crc = dfu_file_write_crc(f, crc, dfusuffix,
        DFU_SUFFIX_LENGTH - 4);*/
        dfusuffix[12] = crc;
        dfusuffix[13] = crc >> 8;
        dfusuffix[14] = crc >> 16;
        dfusuffix[15] = crc >> 24;
        crc = dfu_file_write_crc(f, crc, dfusuffix +
        12, 4);
    }
  •  
  1. Build libusb
  • mkdir -p build
    cd libusb-1.0.24
    ./autogen.sh
    PKG_CONFIG_PATH=$PWD/../build/lib/pkgconfig ./configure --host=x86_64-w64-mingw32 --prefix=$PWD/../build
    make
    make install
    cd ..
  1. Build dfu-util
  • cd dfu-util-0.11
    ./autogen.sh
    PKG_CONFIG_PATH=$PWD/../build/lib/pkgconfig ./configure --host=x86_64-w64-mingw32 --prefix=$PWD/../build
    make
    make install
    cd ..

After these steps, the newly built tool will be located in the /build/bin folder.

Gavin_Jia_0-1733384039454.png

 

Open cmd for Windows. Run the following command with the new dfu-suffix.exe and CRC32 will be added to the Firmware.

dfu-suffix.1 exe -a your_Firmware

Gavin_Jia_1-1733384039494.png

 

Running the Demo

Using Prebuilt Firmware from SDK

The SDK provides a prebuilt Firmware binary (dev_hid_mouse_bm.bin) that already includes CRC32. Follow these steps:

  1. Use MCUXpresso IDE to flash the dev_dfu_freertos_cm7 demo to the EVKB board.
  • Gavin_Jia_2-1733384039655.png

     

  •  
  1. Connect the board to the Host PC via USB.
  • Gavin_Jia_3-1733384039682.png

     

  1. In the USB Device Descriptor, we find the Vendor ID and Product ID:
  • Gavin_Jia_4-1733384039793.png

     

  •  
  1. Run the following command to download the Firmware:
  • dfu-util.exe -d <your_vid:pid> -D <your_Firmware>

After downloading, the DFU demo will verify the CRC32 and execute the new Firmware in RAM. The device will be enumerated as a USB mouse, moving in a rectangular pattern on the screen.

Using Custom Firmware

When using custom Firmware, ensure that the image is loaded at the correct address (e.g., 0x10000). If the offset is incorrect, the DFU demo will fail to load the Firmware, even if the CRC check passes.

Gavin_Jia_5-1733384039909.png

 

To build and load custom Firmware:

  1. Import the hello_world_cm7 project into MCUXpresso IDE.
  2. In the Managed Linker Script settings, enable "Link application to RAM".
  • Gavin_Jia_6-1733384040028.png

     

  1. Adjust memory settings to match the DFU project requirements, ensuring ITCM is the first RAM region.
  • Gavin_Jia_7-1733384040294.png

     

  1. Build the project and generate a binary file.
  • Gavin_Jia_8-1733384040455.png

     

Use the modified dfu-util tool to append CRC32 to the binary and download it to the board. Verify that the custom Firmware executes correctly.

  • CRC Added:
  • Gavin_Jia_9-1733384040480.png

     

  • New Firmware loaded successfully:
  • Gavin_Jia_10-1733384040568.png

     

For Chinese version and demo, please check this link: 
https://www.nxpic.org.cn/module/forum/forum.php?mod=viewthread&tid=803149&fromuid=3253523

ラベル(1)
添付
100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎12-05-2024 12:50 AM
更新者: