Shared Flash Booting for Multi-i.MX RT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Shared Flash Booting for Multi-i.MX RT

Shared Flash Booting for Multi-i.MX RT

1. Backgroud

Customers adopting multi-i.MXRT master-slave architectures (one master, multiple slaves) aim to meet functional requirements while simultaneously reducing costs and improving system efficiency through optimized hardware design.

2.  Multi-i.MXRT Architecture Design

2.1 Independent Flash Architecture (Master-Slave)

In multi-i.MXRT systems, a typical design adopts a master-slave architecture where one i.MXRT acts as the master and others as slaves. Since the i.MXRT chip lacks on-chip non-volatile memory, each i.MXRT requires an independent boot device (e.g., NOR Flash connected via FlexSPI) to load programs and initiate startup. 

Traditional Architecture:

- Each i.MXRT has its own dedicated Flash memory, ensuring operational independence.

Sam_Gao_0-1750324582842.png

Advantages:

- Full System Independence:

  • Each i.MXRT operates independently with its own firmware and boot configuration.
  • Fault isolation: A failure in one Flash or i.MXRT does not affect others.

- Simplified Firmware Management:

  • Independent firmware updates for each i.MXRT without coordination.
  • Easier OTA version control (each device has its own update path).


Disadvantages:
- Complex programming workflow (multiple Flash devices need individual firmware updates).
- Higher hardware complexity, larger PCB footprint, and increased cost due to multiple Flash chips.

2.2 Shared Flash Architecture (Master-Slave with Flash Sharing)

A single Flash device is connected to multiple i.MXRTs. The master i.MXRT controls the POR_B (Power-On Reset) signal of all slave i.MXRTs, enabling shared access to the same Flash.

Boot Process:
1. The master i.MXRT boots first in Non-XIP mode.
2. The master sequentially releases the POR_B signals of slave i.MXRTs, allowing them to occupy the Flash and boot in Non-XIP mode one at a time.

Sam_Gao_1-1750324650518.png

Advantages:
- Reduced cost and simplified hardware design.
- Smaller PCB footprint with only one Flash required.
- Streamlined firmware programming (single Flash update) for mass production.

Disadvantages:
- If slave i.MXRTs require different firmware, the Flash must be partitioned into regions, leading to:
- Complex OTA version management challenges.
- Reduced system independence among slave devices.

3. Hardware Platform Setup

  • Master Board: MIMXRT1010-EVK
  • Slave Board: MIMXRT1010-EVK

Rework:

  • Remove U13 (Flash) from the slave board.
  • Retain U13 on the master board and fly-wire it to U13 of the slave board (only CS, SCLK, IO0, IO1 are required for low-speed boot).
  • Connect GPIO_11 signal of the master i.MXRT1010 to POR_B of the slave i.MXRT1010 (Pin3/4 of SW3).
Sam_Gao_0-1750234973021.png

 


4. Software Design

Due to both master and slave i.MXRTs sharing a single application (differentiated via conditional branches), the app must be Non-XIP. Therefore, we designed a boot_loader project that copies and jumps to the boot_app, instead of using SPT or MCUBootUtility.

Key modules:

  • /boards/evkmimxrt1010/demo_apps/boot_loader
  • /boards/evkmimxrt1010/demo_apps/boot_app
.
├── boards
│   └── evkmimxrt1010
│		├── demo_apps
│		│   ├── boot_app
│		│   ├── boot_loader
│		│   ├── hello_world
│		│   └── led_blinky
│		└── xip
│			├── evkmimxrt1010_flexspi_nor_config.c
│			└── evkmimxrt1010_flexspi_nor_config.h
├── CMSIS
│   ├── Core
│   ├── Driver
│   ├── DSP
│   ├── LICENSE.txt
│   ├── NN
│   └── RTOS2
├── components
│   ├── lists
│   ├── serial_manager
│   └── uart
├── devices
│   └── MIMXRT1011
├── LICENSE
└── README.md

Note: Please see the whole reference project from attchement. 


4.1 boot_loader Design

The boot_loader is a XiP project directly booted by the chip's BootROM. It can be based on the SDK's hello_world example (flexspi_nor target). The FCB boot header should be modified as follows (1-bit SPI, 30MHz, Normal Read Mode):

// boot_loader
// xip/evkmimxrt1010_flexspi_nor_config.c

const flexspi_nor_config_t qspiflash_config = {
    .tag = FLEXSPI_CFG_BLK_TAG,
    .version = FLEXSPI_CFG_BLK_VERSION,
    .readSampleClksrc=kFlexSPIReadSampleClkLoopbackInternally,
    .csHoldTime = 3u,
    .csSetupTime = 3u,
    .deviceType = kFlexSpiDeviceTypeSerialNOR,
    .sflashPadType = kSerialFlash_1Pad,
    .serialClkFreq = kFlexSpiSerialClk_30Hz,
    .sflashA1Size = 16u * 1024u * 1024u,
    .lookupTable = {
        // Read LUTs
        FLEXSPI_LUT_SEQ(CHIP_SELECT, FLEXSPI_1PAD, 0x03, RADDR_SDR, FLEXSPI_1PAD, 0x18),
        FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_1PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0),
    },
    .pageSize = 256u,
    .sectorSize = 4u * 1024u,
    .blockSize = 64u * 1024u,
    .isUniformBlockSize = false,
};

The boot_app is a Non-XIP project (based on SDK’s debug target). Its binary is imported into the boot_loader project. With proper linking address and memory layout, the copy & jump logic can be implemented with standard code. The finalized boot_loader can then be downloaded to Flash using an IDE.


4.2 boot_app Design

The boot_app is also derived from the SDK's hello_world. It supports receiving simple UART commands (A, B, etc.) for various tests. Currently, six test commands are supported: 

Commands Target Device i.MX RT Description
'A' Master Drive master i.MXRT's GPIO_11 high to pull POR_B high and release slave i.MXRT from reset.
'B' Master Drive master i.MXRT's GPIO_11 low to pull POR_B low and hold slave i.MXRT in reset.

 

Commands Target Device Description
'F' Salve Toggle GPIO_11 periodically with a timer to blink the D25 LED.

 

Commands Target Device Description
'C' Master or Slave  Initialize Flash-related pins for FlexSPI functionality.
'D' Master or Slave  Restore Flash-related pins to default GPIO state.
'E' Master or Slave  Erase, program, and read U13 Flash.

 

Notes:

  • Commands A and E may cause conflicts when both master and slave i.MXRT attempt to drive the same Flash through FlexSPI pins. Before executing Command A (to release the slave), the master should first execute Command D, calling the following function to restore FlexSPI pins to GPIO mode. Otherwise, the slave may fail to boot normally (BootROM configures these pins as FlexSPI during boot).
void bsp_deinit_flexspi_pins(void) {
    IOMUXC_SetPinMux(IOMUXC_GPIO_SD_06_GPIO2_IO06, 0U);
    IOMUXC_SetPinMux(IOMUXC_GPIO_SD_07_GPIO2_IO07, 0U);
    IOMUXC_SetPinMux(IOMUXC_GPIO_SD_09_GPIO2_IO09, 0U);
    IOMUXC_SetPinMux(IOMUXC_GPIO_SD_10_GPIO2_IO10, 0U);
    IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_06_GPIO2_IO06, 0x10A0U);
    IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_07_GPIO2_IO07, 0x10A0U);
    IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_09_GPIO2_IO09, 0x10A0U);
    IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_10_GPIO2_IO10, 0x10A0U);
}
  • Commands C and E are typically used together. If the slave has already executed them and remains active, the master must either:
    • The Master execute Command B to reset the slave which resets FlexSPI pin configurations
    • The Slave to execute Command D before running C/E.

5. On-Board Testing

  1. Power up both boards.
  2. Download the boot_loader (containing embedded boot_app) to Flash.

Quick Test:

  1. Sending Command A initially may not start the slave properly.
  2. However, after executing Command D followed by Command A, the slave boots successfully.
  3. Both master and slave boards can read/write the shared Flash normally, verifying the feasibility of this innovative shared flash boot method.Sam_Gao_1-1750239829328.png

Sam_Gao_2-1750239858597.png

Note: Please see readme.md from attchement for more details.

6. Conclusion

The i.MXRT master-slave architectures (Independent Flash vs. Shared Flash) offer distinct trade-offs:
- Independent Flash: Prioritizes system reliability and independent firmware management at the cost of higher hardware complexity and cost.
- Shared Flash: Reduces costs and PCB footprint but introduces firmware dependency and OTA management challenges.

The prototype successfully validated the Shared Flash approach, demonstrating its feasibility for cost-sensitive, mass-production scenarios. Customers can choose between these designs based on their specific priorities: high reliability with independence (Independent Flash) or cost-efficiency with streamlined workflows (Shared Flash).

附件
无评分
版本历史
最后更新:
‎06-19-2025 02:18 AM
更新人: