Application Note (AN12765): DSP Enablement for i.MX RT600 MCUs - XOS Use Cases

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Application Note (AN12765): DSP Enablement for i.MX RT600 MCUs - XOS Use Cases

Application Note (AN12765): DSP Enablement for i.MX RT600 MCUs - XOS Use Cases

The i.MX RT600 MCU includes a Cadence® Tensilica® HiFi 4 DSP running at frequencies of up to 600 MHz.The XOS embedded kernel from Cadence is designed for efficient operation on embedded system built using the Xtensa architecture. Although various parts of XOS continue to be tuned for efficient performance on the Xtensa hardware, most of the code is written in standard C and is not Xtensa-specific.

Click here to access the full application note.

标签 (1)
无评分
版本历史
最后更新:
‎03-05-2020 12:55 PM
更新人: