yocto toolchain problem: missing headers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

yocto toolchain problem: missing headers

跳至解决方案
2,763 次查看
marshall123
Contributor II

Dear Community

i meet problems installing the meta-toolchain in my computer.the system suggested that i successfully installed the toolchain

pastedImage_1.png

but when i use the toolchain it just said that the headers are not inculded

pastedImage_2.png

then i found the header directory is ignored because of "nonexistent" but thet do exist in my computer and is exactly the same name as the directory which is ignored.

pastedImage_3.png

can you help me solve the problem?

if i use the adt-installer, i will meet the same problem.

标签 (2)
0 项奖励
回复
1 解答
2,412 次查看
marshall123
Contributor II

well, I solved it by using $CC to do the compile

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,412 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

   Please look at the following :

https://community.nxp.com/thread/394804 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 项奖励
回复
2,412 次查看
marshall123
Contributor II

nope, I don't think it solved the problem, it may because the headers is not linked to the tool chain.

I want to know how to link it to the toolchain.

or every time i have to use the script to run the toolchain.and the other headers may be also missing.

0 项奖励
回复
2,412 次查看
Yuri
NXP Employee
NXP Employee

Please look at the following :

https://community.nxp.com/docs/DOC-173488 

Regards,

Yuri.

0 项奖励
回复
2,413 次查看
marshall123
Contributor II

well, I solved it by using $CC to do the compile

0 项奖励
回复