yocto project and development for my our i.MX6 system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

yocto project and development for my our i.MX6 system

1,105 次查看
misbahk
Contributor I

Hi All,

I am using the fsl yocto project for building my own system using the standard kernel + uboot + filesystem from freescale and adding + modifying the BSP from Freescale.

I am new to yocto but would like to use it and maintain it for future projects and development.

How can i have my own customized BSP from freescale and use it under yocto project.

Reference documentation and study material where can i find. Please suggest.

I would also need, the same yocto project to build ubuntu image or may be Android image using the same kernel and u-boot of mine customized from freescale.

Making use of the yocto's capability.

Please suggest and guide in this direction. Also share with the study material + your guidance and supporting documents to achieve and do the thing in the best possible way and use the yocto the best possible way.

Regards,

Misbah

0 项奖励
回复
1 回复

933 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Please use the next Community link regarding Yocto approach. 

i.MX Yocto Project: Frequently Asked Questions


General information may be found at

https://www.yoctoproject.org/tools-resources/community

Also, please refer to “Freescale_Yocto_Project_User's_Guide.pdf” in BSP docs :

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复