yocto: no build of the DRI part in xserver-xorg-video-imx-viv ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto: no build of the DRI part in xserver-xorg-video-imx-viv ?

650件の閲覧回数
thierrybultel
Contributor II

Hi,

The libdri.so, which is expected by X at /usr/lib/xorg/modules/extensions/libdri.so,

is not built. It is normally built by the DRI part of xerver-xorg-video-imx-viv.

Only the EXA part is done.

Hacking to make it built makes some compilation errors, with xserver version 1.14

(though it worked fine with xserver 1.12)

Is there a patch somewhere, or does that mean that libdri.so should not be needed ?

Regards

Thierry

0 件の賞賛
返信
1 返信

476件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Which Yocto BSP are you using? The community BSP or the BSP Release?

Unfortunately there is no patch available that I know of but dizzy should work for xserver 1.14, although the driver used is vivante_dri.

Have you baked the following package?

bitbake xf86-video-imxfb-vivante

0 件の賞賛
返信