yocto mono layer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

yocto mono layer

2,686 次查看
tüskemáté
Contributor I

   Hi,

I'm working on a system where i can run c# applications in raspberry pi. I'm just switched to yocto rocko, and somehow now I always fail on the do_package_qa task. This is my error message:

ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Engine.dll contained in package mono-libs-3.5 requires mono(System.Xml), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Utilities.v3.5.dll contained in package mono-libs-3.5 requires mono(System), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Engine.dll contained in package mono-libs-3.5 requires mono(mscorlib), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(mscorlib), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System.Xml), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System.Configuration), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(Mono.Security), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6.2-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6.2 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6.2? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.7-api/Mono.Debugger.Soft.dll contained in package mono-api-4.7 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.7? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/xbuild/Microsoft/NuGet/Microsoft.NuGet.Build.Tasks.dll contained in package mono-xbuild requires mono(mscorlib), but no providers found in RDEPENDS_mono-xbuild? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6.1-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6.1 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6.1? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/gac/Mono.Messaging.RabbitMQ/4.0.0.0__0738eb9f132ed756/Mono.Messaging.RabbitMQ.dll contained in package mono-gac requires mono(mscorlib), but no providers found in RDEPENDS_mono-gac? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.5/Microsoft.CodeAnalysis.Scripting.dll contained in package mono-libs-4.5 requires mono(System.Runtime.Loader), but no providers found in RDEPENDS_mono-libs-4.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA run found fatal errors. Please consider fixing them. 
ERROR: mono-5.4.1.6-r0 do_package_qa: Function failed: do_package_qa

My mono version is 5.8.0.108 from http://download.mono-project.com/repo/ubuntu  and I'm using xenial ubuntu. The local.conf is now the sample from here:https://git.yoctoproject.org/cgit.cgi/poky/plain/meta-poky/conf/local.conf.sample . 

Any suggestion?

regards

Matthew

标签 (1)
标记 (3)
2 回复数

2,032 次查看
a_spin
Contributor I

I'm experiencing the same problem.

Did this document solve you're problem, I didn't find a clue in it.

Regards,

Alberto

0 项奖励
回复

2,032 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Matthew,

The Mono layer is not present on the i.MX BSPs so I’m not familiar with it, but there seems to be problems with dependencies for adding mono. If you are using Yocto perhaps the following document on the Yocto Project Wiki may help.

https://wiki.yoctoproject.org/wiki/Building_and_running_embedded_Linux_.NET_applications_from_first_...

Regards,