[yocto][linux-imx to linux-fslc] CLK01 activation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[yocto][linux-imx to linux-fslc] CLK01 activation

1,456 Views
aurele
Contributor I


Hi everyone,

 

I'm using a board equiped with IMX6 dual Lite, with codec sgtl5000, clk01 (on GPIO_0) is used as master clock for the sgtl5000.

The build system is yocto on branch krogoth

With linux-imx, everything was fine.

then I switched to Linux-fslc, now the sgtl5000 is not detected anymore, I could see that the clock is not generated anymore...

I checked the i2c control signals, everything is fine on the bus, but as the master clock is not available, the chip doesn't answer...

So now the sgtl 5000 is not detected anymore on the I2C bus

 

My question is :

How can I get this clock generated/activated? maybe something is missing in my devicetree but as I didn't modified it I don't know what it could be.

 

Thanks for any help

Aurele

 

 

I joined the content of /sys/kernel/debug/clk/clk_summary file. I saw that CKO clocks are not active at all

 

below some pieces of my devicetree :

 

&i2c2 {

  status = "okay";

  clock-frequency = <100000>;

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_i2c2_moniteur>;

  codec: sgtl5000@0a {

  compatible = "fsl,sgtl5000";

  reg = <0x0a>;

  clocks = <&clks 201>;

  VDDA-supply = <&reg_3p3v>;

  VDDIO-supply = <&reg_3p3v>;

  };

};

 

&ssi1 {

  fsl,mode = "i2s-slave";

  status = "okay";

};

 

sound {

  compatible = "fsl,imx6dl-moniteur-sgtl5000", "fsl,imx-audio-sgtl5000";

  model = "imx6dl-moniteur-sgtl5000";

  ssi-controller = <&ssi1>;

  audio-codec = <&codec>;

  audio-routing =

  "MIC_IN", "Mic Jack",

  "Mic Jack", "Mic Bias",

  "Headphone Jack", "HP_OUT";

  mux-int-port = <1>;

  mux-ext-port = <3>;

  };

 

in iomuxc section :

pinctrl_moniteur: moniteurgrp {

  fsl,pins = <

  MX6QDL_PAD_GPIO_0__CCM_CLKO1    0x130b0 /* SGTL5000 sys_mclk */

  MX6QDL_PAD_NANDF_D0__GPIO2_IO00    0x80000000 /* BP0 */

  MX6QDL_PAD_NANDF_D1__GPIO2_IO01    0x80000000 /* BP1 */

  MX6QDL_PAD_NANDF_D2__GPIO2_IO02    0x80000000 /* BP2 */

  MX6QDL_PAD_NANDF_D3__GPIO2_IO03    0x80000000 /* BP3 */

 

 

  MX6QDL_PAD_GPIO_3__GPIO1_IO03    0x80000000 /* Reset DSP */

  MX6QDL_PAD_GPIO_8__GPIO1_IO08    0x80000000 /* Mute Ampli HP */

  MX6QDL_PAD_GPIO_9__GPIO1_IO09    0x80000000 /* Mute Ampli Loop */

 

 

  >;

  };

pinctrl_i2c2_moniteur: i2c2grp-moniteur {

  fsl,pins = <

  MX6QDL_PAD_KEY_COL3__I2C2_SCL 0x4001b8b1

  MX6QDL_PAD_KEY_ROW3__I2C2_SDA 0x4001b8b1

  >;

  };

 

 

root@MON100003:~# cat /sys/kernel/debug/clk/clk_summary   clock                         enable_cnt  prepare_cnt        rate   accuracy   phase---------------------------------------------------------------------------------------- anaclk2                                  0            0           0          0 0      lvds2_in                              0            0           0          0 0   anaclk1                                  0            0           0          0 0      lvds1_in                              0            0           0          0 0   dummy                                    3            4           0          0 0      lvds2_sel                             0            0           0          0 0         lvds2_gate                         0            0           0          0 0      usbphy2_gate                          1            1           0          0 0      usbphy1_gate                          1            1           0          0 0   osc                                      6            6    24000000          0 0      cko2_sel                              0            0    24000000          0 0         cko2_podf                          0            0    24000000          0 0            cko2                            0            0    24000000          0 0               cko                          0            0    24000000          0 0      periph_clk2_sel                       0            0    24000000          0 0         periph_clk2                        0            0    24000000          0 0      gpt_3m                                1            1     3000000          0 0      pll7_bypass_src                       1            1    24000000          0 0         pll7                               1            1   480000000          0 0            pll7_bypass                     1            1   480000000          0 0               pll7_usb_host                1            1   480000000          0 0                  usbphy2                   1            1   480000000          0 0      pll6_bypass_src                       1            1    24000000          0 0         pll6                               1            1   500000000          0 0            pll6_bypass                     1            1   500000000          0 0               pll6_enet                    1            1   500000000          0 0                  enet_ref                  1            1    50000000          0 0                  pcie_ref                  0            0   125000000          0 0                     pcie_ref_125m           0            0   125000000          0 0                  sata_ref                  0            0   100000000          0 0                     sata_ref_100m           0            0   100000000          0 0                        lvds1_sel           0            0   100000000          0 0                           lvds1_gate           0            0   100000000          0 0      pll5_bypass_src                       0            0    24000000          0 0         pll5                               0            0   296600000          0 0            pll5_bypass                     0            0   296600000          0 0               pll5_video                   0            0   296600000          0 0                  pll5_post_div             0            0    74150000          0 0                     pll5_video_div           0            0    74150000          0 0                        ipu2_di1_pre_sel           0            0    74150000          0 0                           ipu2_di1_pre           0            0    37075000          0 0                              ipu2_di1_sel           0            0    37075000          0 0                                 ipu2_di1           0            0    37075000          0 0                        ipu2_di0_pre_sel           0            0    74150000          0 0                           ipu2_di0_pre           0            0    24716667          0 0                              ipu2_di0_sel           0            0    24716667          0 0                                 ipu2_di0           0            0    24716667          0 0                        ipu1_di1_pre_sel           0            0    74150000          0 0                           ipu1_di1_pre           0            0    24716667          0 0                              ipu1_di1_sel           0            0    24716667          0 0                                 ipu1_di1           0            0    24716667          0 0                        ipu1_di0_pre_sel           0            0    74150000          0 0                           ipu1_di0_pre           0            0    24716667          0 0                              ipu1_di0_sel           0            0    24716667          0 0                                 ipu1_di0           0            0    24716667          0 0                        ldb_di1_sel           0            0    74150000          0 0                           ldb_di1_div_7           0            0    10592857          0 0                              ldb_di1_div_sel           0            0    10592857          0 0                                 ldb_di1           0            0    10592857          0 0                           ldb_di1_div_3_5           0            0    21185714          0 0                        ldb_di0_sel           0            0    74150000          0 0                           ldb_di0_div_7           0            0    10592857          0 0                              ldb_di0_div_sel           0            0    10592857          0 0                                 ldb_di0           0            0    10592857          0 0                           ldb_di0_div_3_5           0            0    21185714          0 0      pll4_bypass_src                       0            0    24000000          0 0         pll4                               0            0   147456000          0 0            pll4_bypass                     0            0   147456000          0 0               pll4_audio                   0            0   147456000          0 0                  pll4_post_div             0            0    36864000          0 0                     pll4_audio_div           0            0    36864000          0 0      pll3_bypass_src                       1            1    24000000          0 0         pll3                               1            1   480000000          0 0            pll3_bypass                     1            1   480000000          0 0               pll3_usb_otg                 3            4   480000000          0 0                  periph2_clk2_sel           0            0   480000000          0 0                     periph2_clk2           0            0   480000000          0 0                  asrc_sel                  0            0   480000000          0 0                     asrc_pred              0            0   240000000          0 0                        asrc_podf           0            0    30000000          0 0                           asrc             0            0    30000000          0 0                  esai_sel                  0            0   480000000          0 0                     esai_pred              0            0   240000000          0 0                        esai_podf           0            0    30000000          0 0                           esai_extal           0            0    30000000          0 0                  pll3_60m                  0            1    60000000          0 0                     can_root               0            0    30000000          0 0                        can2_serial           0            0    30000000          0 0                        can1_serial           0            0    30000000          0 0                     ecspi_root             0            1    60000000          0 0                        ecspi4              0            0    60000000          0 0                        ecspi3              0            0    60000000          0 0                        ecspi2              0            2    60000000          0 0                        ecspi1              0            0    60000000          0 0                  pll3_80m                  1            1    80000000          0 0                     uart_serial_podf           1            1    80000000          0 0                        uart_serial           2            3    80000000          0 0                  pll3_120m                 0            0   120000000          0 0                  pll3_pfd3_454m            0            0   454736842          0 0                     spdif_sel              0            0   454736842          0 0                        spdif_pred           0            0   227368421          0 0                           spdif_podf           0            0    28421053          0 0                              spdif           0            0    28421053          0 0                  pll3_pfd2_508m            0            0   508235294          0 0                     ssi3_sel               0            0   508235294          0 0                        ssi3_pred           0            0   127058824          0 0                           ssi3_podf           0            0    63529412          0 0                              ssi3           0            0    63529412          0 0                     ssi2_sel               0            0   508235294          0 0                        ssi2_pred           0            0   127058824          0 0                           ssi2_podf           0            0    63529412          0 0                              ssi2           0            0    63529412          0 0                     ssi1_sel               0            0   508235294          0 0                        ssi1_pred           0            0   127058824          0 0                           ssi1_podf           0            0    63529412          0 0                              ssi1           0            0    63529412          0 0                  pll3_pfd1_540m            2            2   540000000          0 0                     axi_alt_sel            1            1   540000000          0 0                        axi_sel             1            1   540000000          0 0                           axi              2            2   270000000          0 0                              openvg_axi           0            0   270000000          0 0                              vpu_axi_sel           0            0   270000000          0 0                                 vpu_axi_podf           0            0   270000000          0 0                                    vpu_axi           0            0   270000000          0 0                              vdo_axi_sel           0            0   270000000          0 0                                 vdo_axi           0            0   270000000          0 0                                    vdoa           0            0   270000000          0 0                              emi_slow_sel           1            1   270000000          0 0                                 emi_slow_podf           1            1   135000000          0 0                                    eim_slow           2            2   135000000          0 0                              pcie_axi_sel           0            0   270000000          0 0                                 pcie_axi           0            0   270000000          0 0                     ipu1_sel               1            1   540000000          0 0                        ipu1_podf           1            1   270000000          0 0                           ipu1             2            2   270000000          0 0                              ipu1_pclk1_sel           0            0   270000000          0 0                                 ipu1_pclk1_div           0            0           0          0 0                                    ipu1_pclk_1           0            0           0          0 0                              ipu1_pclk0_sel           1            1   270000000          0 0                                 ipu1_pclk0_div           1            1    27000000          0 0                                    ipu1_pclk_0           1            1    27000000          0 0                           dcic1            0            0   270000000          0 0                     hdmi_isfr              0            0   540000000          0 0                     video_27m              0            0    27000000          0 0                  pll3_pfd0_720m            0            0   720000000          0 0                  usbphy1                   0            0   480000000          0 0      pll2_bypass_src                       1            1    24000000          0 0         pll2                               1            1   528000000          0 0            pll2_bypass                     1            1   528000000          0 0               pll2_bus                     1            1   528000000          0 0                  pll2_pfd2_396m            1            1   396000000          0 0                     enfc_sel               0            0   396000000          0 0                        enfc_pred           0            0    79200000          0 0                           enfc_podf           0            0    19800000          0 0                              enfc           0            0    19800000          0 0                                 gpmi_io           0            0    19800000          0 0                     ipu2_sel               0            0   396000000          0 0                        ipu2_podf           0            0   198000000          0 0                           ipu2             0            0   198000000          0 0                           dcic2            0            0   198000000          0 0                     emi_sel                0            0   396000000          0 0                        emi_podf            0            0   198000000          0 0                     usdhc4_sel             0            0   396000000          0 0                        usdhc4_podf           0            0   198000000          0 0                           usdhc4           0            0   198000000          0 0                              gpmi_bch           0            0   198000000          0 0                     usdhc3_sel             0            0   396000000          0 0                        usdhc3_podf           0            0   198000000          0 0                           usdhc3           0            0   198000000          0 0                              apbh_dma           0            0   198000000          0 0                              per1_bch           0            0   198000000          0 0                              gpmi_bch_apb           0            0   198000000          0 0                              gpmi_apb           0            0   198000000          0 0                     usdhc2_sel             0            0   396000000          0 0                        usdhc2_podf           0            0   198000000          0 0                           usdhc2           0            0   198000000          0 0                     usdhc1_sel             0            0   396000000          0 0                        usdhc1_podf           0            0   198000000          0 0                           usdhc1           0            0   198000000          0 0                     hsi_tx_sel             0            0   396000000          0 0                        hsi_tx_podf           0            0   198000000          0 0                           hsi_tx           0            0   198000000          0 0                     periph2_pre            0            0   396000000          0 0                        periph2             0            0   396000000          0 0                           mmdc_ch1_axi           0            0   396000000          0 0                     periph_pre             1            1   396000000          0 0                        periph              2            2   396000000          0 0                           mmdc_ch0_axi           1            1   396000000          0 0                              gpu3d_axi           0            0   396000000          0 0                              gpu2d_axi           0            0   396000000          0 0                           ahb              6            7   132000000          0 0                              sdma           8            2   132000000          0 0                              sata           0            0   132000000          0 0                              rom           1            1   132000000          0 0                              ocram           2            2   132000000          0 0                              hdmi_iahb           0            0   132000000          0 0                              esai_mem           0            0   132000000          0 0                              esai_ipg           0            0   132000000          0 0                              caam_aclk           1            1   132000000          0 0                              caam_mem           1            1   132000000          0 0                              asrc_mem           0            0   132000000          0 0                              asrc_ipg           0            1   132000000          0 0                              cko1_sel           0            0   132000000          0 0                                 cko1_podf           0            0    16500000          0 0                                    cko1           0            0    16500000          0 0                              ipg           5            6    66000000          0 0                                 usboh3           0            0    66000000          0 0                                 uart_ipg           2            3    66000000          0 0                                 ssi3_ipg           0            0    66000000          0 0                                 ssi2_ipg           0            0    66000000          0 0                                 ssi1_ipg           0            1    66000000          0 0                                 spdif_gclk           0            0    66000000          0 0                                 spba           0            0    66000000          0 0                                 iim           0            0    66000000          0 0                                 gpt_ipg           1            1    66000000          0 0                                 enet           2            2    66000000          0 0                                 can2_ipg           0            0    66000000          0 0                                 can1_ipg           0            0    66000000          0 0                                 caam_ipg           1            1    66000000          0 0                                 ipg_per           1            1    66000000          0 0                                    pwm4           0            0    66000000          0 0                                    pwm3           0            0    66000000          0 0                                    pwm2           0            0    66000000          0 0                                    pwm1           1            1    66000000          0 0                                    i2c3           0            0    66000000          0 0                                    i2c2           0            0    66000000          0 0                                    i2c1           0            0    66000000          0 0                                    gpt_ipg_per           0            0    66000000          0 0                                    i2c4           0            0    66000000          0 0                     step                   0            0   396000000          0 0                     pll2_198m              0            0   198000000          0 0                  pll2_pfd1_594m            0            0   528000000          0 0                     gpu3d_shader_sel           0            0   528000000          0 0                        gpu3d_shader           0            0   528000000          0 0                           gpu2d_core           0            0   528000000          0 0                     gpu3d_core_sel           0            0   528000000          0 0                        gpu3d_core_podf           0            0   528000000          0 0                           gpu3d_core           0            0   528000000          0 0                  pll2_pfd0_352m            0            0   306580645          0 0                     gpu2d_core_sel           0            0   306580645          0 0                        gpu2d_core_podf           0            0   153290323          0 0                           mlb              0            0   153290323          0 0      pll1_bypass_src                       1            1    24000000          0 0         pll1                               1            1   996000000          0 0            pll1_bypass                     1            1   996000000          0 0               pll1_sys                     1            1   996000000          0 0                  pll1_sw                   1            1   996000000          0 0                     arm                    1            1   996000000          0 0                        twd                 0            0   498000000          0 0   ckih1                                    0            0           0          0 0   ckil                                     0            0       32768          0 0 

Original Attachment has been moved to: clk_summary.zip

Labels (3)
0 Kudos
Reply
1 Reply

1,109 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aurele

Linux-fslc is supported by community

https://community.freescale.com/message/402940#402940

one can post it on meta-fsl-arm mailing list, so that someone familiar

with it could try to assist you

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply