hai sir,
i need to do yocto build for beagle bone board.
I followed the below steps for downloading the yocto source code Task #1 - Download the source code .
Then i change the build /conf/local.conf file
MACHINE ??= 'beaglebone'
then i build bitbake core-image-sato-sdk
i get an error like
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
Please set a valid MACHINE in your local.conf or environment
ERROR: Execution of event handler 'check_sanity_eventhandler' failed
ERROR: Command execution failed: Exited with 1
could you please help me to resolve this issue,This is an urgent issue.
regards
Sachu
Hi,
The beaglebone board is not included in the FSL BSP. Therefore it is expected to have an error.
You may find this very helpful.
https://www.yoctoproject.org/downloads/bsps/daisy16/beaglebone
Best Regards,
Alejandro