Hi ,
I am getting these following errors when i do bitbake armnn ,
Sstate summary: Wanted 28 Found 6 Missed 22 Current 3663 (21% match, 99% complete)
NOTE: Executing Tasks
ERROR: armnn-19.08-r1 do_prepare_recipe_sysroot: The file /usr/lib/libneuralnetworks.so is installed by both imx-gpu-viv and nn-imx, aborting
ERROR: Logfile of failure stored in: /home/sarath/agljellyfish/build/tmp/work/aarch64-agl-linux/armnn/19.08-r1/temp/log.do_prepare_recipe_sysroot.5367
ERROR: Task (/home/sarath/agljellyfish/bsp/meta-imx/meta-ml/recipes-libraries/armnn/armnn_git.bb:do_prepare_recipe_sysroot) failed with exit code '1'
NOTE: Tasks Summary: Attempted 5521 tasks of which 5520 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/sarath/agljellyfish/bsp/meta-imx/meta-ml/recipes-libraries/armnn/armnn_git.bb:do_prepare_recipe_sysroot
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.