software: L3.10.53-1.1.0-GA
error log file:
tmp/work/cortexa9hf-vfp-neon-mx6-poky-linux-gnueabi/imx-gpu-viv/1_5.0.11.p4.1-hfp-r0/temp/log.do_unpack.16594
DEBUG: Executing python function do_unpack
NOTE: Freescale EULA has been accepted for 'imx-gpu-viv'
DEBUG: Executing python function base_do_unpack
NOTE: Unpacking /media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/downloads/imx-gpu-viv-5.0.11.p4.1-hfp.bin to /media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/build-x11/tmp/work/cortexa9hf-vfp-neon-mx6-poky-linux-gnueabi/imx-gpu-viv/1_5.0.11.p4.1-hfp-r0/
DEBUG: Python function base_do_unpack finished
DEBUG: Executing python function fsl_bin_do_unpack
NOTE: Handling file 'imx-gpu-viv-5.0.11.p4.1-hfp.bin' as a Freescale's EULA binary.
DEBUG: Running export SSH_AGENT_PID="2552"; export SSH_AUTH_SOCK="/tmp/keyring-680Bhd/ssh"; export PATH="/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/sources/poky/scripts:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/build-x11/tmp/sysroots/x86_64-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/build-x11/tmp/sysroots/imx6qsabresd/usr/bin/crossscripts:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/build-x11/tmp/sysroots/x86_64-linux/usr/sbin:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/build-x11/tmp/sysroots/x86_64-linux/usr/bin:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/build-x11/tmp/sysroots/x86_64-linux/sbin:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/build-x11/tmp/sysroots/x86_64-linux/bin:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/sources/poky/scripts:/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/sources/poky/bitbake/bin:/home/kevin/kevin-acce/:/home/kevin/bin/:/media/tools/android/android-studio/bin:/usr/lib/gradle-2.4/bin:/usr/lib/jvm/jdk1.7.0_72//bin:/home/kevin/MentorGraphics/Sourcery_CodeBench_Lite_for_ARM_EABI/bin:/home/kevin/CodeSourcery/Sourcery_G++_Lite/bin:/home/kevin/kevin-acce/:/home/kevin/bin:/usr/local/arm_linux_4.2/bin:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games"; export HOME="/home/kevin"; sh /media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/downloads/imx-gpu-viv-5.0.11.p4.1-hfp.bin --auto-accept --force
ERROR: Error executing a python function in /media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/imx-gpu-viv/imx-gpu-viv_5.0.11.p4.1-hfp.bb:
The stack trace of python calls that resulted in this exception/failure was:
File: 'fsl_bin_do_unpack', lineno: 35, function: <module>
0031: # Return to the previous directory
0032: os.chdir(save_cwd)
0033:
0034:
*** 0035:fsl_bin_do_unpack(d)
0036:
File: 'fsl_bin_do_unpack', lineno: 29, function: fsl_bin_do_unpack
0025: save_cwd = os.getcwd()
0026: os.chdir(rootdir)
0027:
0028: cmd = "sh %s --auto-accept --force" % (url.localpath)
*** 0029: bb.fetch2.runfetchcmd(cmd, d, quiet=True)
0030:
0031: # Return to the previous directory
0032: os.chdir(save_cwd)
0033:
File: '/media/UD-SOURCES2/freescale/yocto/3.10.53-1.1.0/L3.10.53-1.1.0-GA/fsl-release-bsp/sources/poky/bitbake/lib/bb/fetch2/__init__.py', lineno: 722, function: runfetchcmd
0718: bb.utils.remove(f, True)
0719: except OSError:
0720: pass
0721:
*** 0722: raise FetchError(error_message)
0723:
0724: return output
0725:
0726:def check_network_access(d, info = "", url = None):
Exception: FetchError: Fetcher failure: Fetch command failed with exit code 15, output:
Welcome to Freescale imx-gpu-viv-5.0.11.p4.1-hfp.bin
WARNING: EULA has been auto-accepted; this imply you agree with it anyway.
Unpacking file ..
mkdir: cannot create directory `imx-gpu-viv-5.0.11.p4.1-hfp': File exists
bzip2: (stdin) is not a bzip2 file.
ERROR:
Signal caught, cleaning up
DEBUG: Python function fsl_bin_do_unpack finished
DEBUG: Python function do_unpack finished
ERROR: Function failed: fsl_bin_do_unpack
my test:
kevin$ sh imx-gpu-viv-5.0.11.p4.1-hfp.bin --auto-accept --force
Welcome to Freescale imx-gpu-viv-5.0.11.p4.1-hfp.bin
WARNING: EULA has been auto-accepted; this imply you agree with it anyway.
Unpacking file bzip2: (stdin) is not a bzip2 file.
..ERROR:
Signal caught, cleaning up
please give me some suggestion about this problem.
It seems the eula file imx-gpu-viv-5.0.11.p4.1-hfp.bin can't install properly!
Hi kevin,
I saw the same error before, but I changed to imx-gpu-viv-5.0.11.p4.4-hfp.bin and it wokrs well under 3.10.53.
Hope this helps