Hi,
I am using imx6q sabresd board.I am trying to build a linux system based on the BSP of L3.0.35_4.1.0_130816_source.tar.gz, and the OS of my host PC is Ubuntu 14.04. But when I built the FSL gnome release package system, I met an error as follows:
configure: error: tslib must be installed to build the tslib input driver.
error: Bad exit status from /home/b54871/i.MX6DQ_SDP/L3.0.35_4.1.0_130816_source/cmh/ltib/tmp/rpm-tmp.79842 (%build)
RPM build errors:
Bad exit status from /home/b54871/i.MX6DQ_SDP/L3.0.35_4.1.0_130816_source/cmh/ltib/tmp/rpm-tmp.79842 (%build)
Build time for xorg-server: 15 seconds
Failed building xorg-server
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed Jun 24 15:35:22 2015
Ended: Wed Jun 24 15:36:12 2015
Elapsed: 50 seconds
These packages failed to build:
xorg-server
Build Failed
Exiting on error or interrupt
Can anybody please help me with this issue?